REGEN.TEST

Description

This command is used to trigger the self-test to ensure the regen resistor has been wired correctly.

Executing REGEN.TEST will put current through the regen resistor circuit and verify bus voltage drops by a percentage (REGEN.TESTVTHRESH) of the initial voltage. If the timeout, (REGEN.TESTTO), is exceeded the test will fail.

REGEN.TESTSTATUS shows the results of the test. If the bus voltage reaches the threshold before the timeout, everything is considered correct and the test passes. If a short circuit is present, the test will fail early, and a fault will be present. If an open circuit is present, the test timeout will be surpassed, and the failure is reported in the test status.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REGEN.TESTTO,

REGEN.TESTSTATUS,

REGEN.TESTVTHRESH

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TEST

2406

966

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TEST

2406

Unsigned8

Read/Write

-